Victaulic Vortex™
- Home
- Products
- Special Hazards
- Victaulic Vortex™
Victaulic Vortex is a hybrid fire extinguishing system that provides the best aspects of both water mist and inert gas systems. The system uses inert gas and water to generate a nitrogen-enriched atmosphere that opposes combustion. Browse Victaulic Vortex™ Hybrid Fire Extinguishing Systems listed below. View More
One of the most appealing aspects of the Victaulic Vortex system is the environmentally green design that uses non-toxic agents to keep personnel safe during activation. There is no need to evacuate the room before the system engages or maintain a tight room integrity after the system has deployed.
How Does Hybrid Fire Suppression Work?
In our environment the air already contains 78% percent nitrogen; when a Victaulic Vortex system discharges, the addition of nitrogen dilutes the air and allows the tiny water particles to absorb the heat, creating an atmosphere that does not support combustion. Victaulic Vortex hybrid fire suppression systems efficiently extinguish fires with nearly zero wetting, no expensive clean-up, equipment replacement or profit loss from systems being offline.One of the most appealing aspects of the Victaulic Vortex system is the environmentally green design that uses non-toxic agents to keep personnel safe during activation. There is no need to evacuate the room before the system engages or maintain a tight room integrity after the system has deployed.